Search result

249 machines were found

Matrix Model 0550 CNC External Thread Grinding Machine, exhibited with 'Tap' grinding module. Features of this high precision external thread grinder include a Torque Motor Driven Workhead for conci...
  • Hall: 11
  • Matrix Machine Tool (Coventry) Limited
NEW for 2019 Matrix are pleased to launch the NEW Matrix MVC-0400 5 axis Multi-function CNC Machine for Bevel Gear Cutting, Turning and 'Power Skiving' capabilities. Components up to 400 mm diameter...
  • Hall: 11
  • Matrix Machine Tool (Coventry) Limited
Efficient, high-volume manufacturing of structural parts for electromobility: BA W08-12 The BA W08-12 from SW is specially designed for manufacturing high-volume light metal workpieces for electri...
  • Hall: 12
  • Schwäbische Werkzeugmaschinen GmbH
The NBV 700 MT: Adapts to every machining job. The vertical 5-axis machining center NBV 700 MT offers our customers almost unlimited flexibility in production. The innovative machine concept enables...
  • Hall: 12
  • Hüller-Hille
High Speed and plenty of space: 60 m/min with pallet size 800 x 800 mm for heaviest workpieces. The NBH 800 has large power reserves and ensures safety when extreme cutting forces occur. A sturdy g...
  • Hall: 12
  • Hüller-Hille
MILLING-TURNING CENTER - FROM BLANK TO FINISHED PART IN ONE SET-UP Completely machine difficult to cut and complex workpieces flexibly and productively. One of the key challenges operators&nb...
  • Hall: 12
  • STAMA Maschinenfabrik GmbH
Flexible and Productive Gear Hobbing Machine with Vertical Workpiece Additional equipment is offering the chamfering of teeth with forming or cutting tools. The machine configuration can be design...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Horizontal 5-axis machining center The single-spindle machine SPECHT 700 is widely configurable for use in flexible manufacturing systems. It is individually built in synchronised flow assembly for ...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
VDF DUS universal turning machines with cycle controls are ideal for machining very long parts and high-strength materials at high removal. Numerous options enable individual solutions for every requ...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Fast Bed-Type Milling Machine with Traversing Column
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
This short drilling machine is equipped with a 51 kW main spindle drive, covering a drilling diameter range in steel of 20 - 120 mm. The tools are tightened with a HSK-A100 tool holder inside the mai...
  • Hall: 15
  • Loch Präzisionsbohrtechnik GmbH
Since 1994 Ergo has been Famars flagship machine. Its special characteristic is the technological revolution of the vertical lathe. Born from the technological revolution represented by the vertical ...
  • Hall: 17
  • Famar Srl
Seiger is the only German manufacturer displaying a surface lathe at this trade fair. The lathe is equipped with the Siemens SINUMERIK 840D sl V4.7 control system, which includes manual functions an...
  • Hall: 17
  • Willi Seiger GmbH
The turning-milling machining centers of the CTX TC and CTX TC 4A series represent the premier class of universal turning. Thanks to their counter spindle, they enable 6-sided complete machining. The...
  • Hall: 2
  • DMG MORI
DMP 70 - The perfect answer to the requirements of 3 axis and 5 axis machining for production oriented areas The machine concept of DMP 70 combines highest precision, tremendous rigidity as well a...
  • Hall: 2
  • DECKEL MAHO Seebach GmbH
Designed for exceptionally accurate milling, drilling and rigid tapping. Wide variety of demanding applications including high precision molds and dies The extraordinary stiffness of the col...
  • Hall: 26
  • PING JENG MACHINERY INDUSTRY CO., LTD.
The 260HMS is suited for all gear honing requirements: shafts, workpieces, or small and complex applications. Gear flank modifications can be adjusted even during the manufacturing process via the in...
  • Hall: 26
  • Gleason Sales
The rack measuring machine has a non-contact complete measurement of a rack. The measurement includes individual pitch, cumulative pitch, roll dimension, flank angle, helix angle, perpendicularity, b...
  • Hall: 26
  • HABRAMA GmbH
More clearance, more power, more possibilities: with a spindle distance of 1400 mm, a powerful counter spindle which also allows 4-axis machining and a B-axis with a direct drive for complex 5-axis s...
  • Hall: 27
  • EMCO GmbH
The VTC-800 series of Vertical Machining Centres has been designed to meet the needs for today's challenging and diverse range of manufacturing applications where performance, flexibility and precisi...
  • Hall: 27
  • Yamazaki Mazak

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter