Search result

249 machines were found

With the JIG machine tools, Mikromat provides the world's leading technology for precision processing. Mikromat systems ensure that your precision manufacturing is more precisely, your production mor...
  • Hall: 11
  • Mikromat GmbH
With the WOTAN S3A Series will be presented a compact external cylindrical grinding machine. Thanks to its intelligent machining strategy and the small design, the machine is particularly suitable fo...
  • Hall: 11
  • NSH Group
SPARK 1200 A MULTITASKING COMPACT Maximum static and dynamic stiffness of the electro-welded structures, high torques and rigidity at the rotary table and spindle, highly performing drives. These...
  • Hall: 12
  • Mandelli Sistemi Spa
The CHIRON MILL series is the optimal solution for highly productive cutting and machining applications. Whether your focus is on flexible single-unit production, or high volume precision manufacturi...
  • Hall: 12
  • CHIRON Werke GmbH & Co.KG
Short lead times When you need the flexibility of mill-turn operations on both single part and series production, choose the Uniport 7000-MTC. This multi-task machine achieves extremely short lea...
  • Hall: 13
  • UNISIGN Machine Tools
More productivity More capacity and more clearance in the working envelope the Unicom 7000 is all about achieving more productivity for larger components. Like its brother the Unicom 6000 this ...
  • Hall: 13
  • UNISIGN Machine Tools
COMBINED MILLING AND LATHERING With the spindle clamping and the optional rotary table, workpieces can be turned at a maximum speed of 250 min -1 . The time-consuming exchanging of the workpiec...
  • Hall: 13
  • Reiden Technik AG
ARION G, multitask machining center that combines milling/ turning functions. With the development and incorporation of the latest technologies in its design and manufacture, it has achieved a versa...
  • Hall: 13
  • zayer
The multi-function machine with B axis can easy have bevel angle drilling and cutting work. The B axis is driven by DD build-in motor, the best torque is 3,000 Nm, and with curved coupling ...
  • Hall: 14
  • LEADWELL CNC MACHINES MFG., CORP.
Vertical Turning Machine Compact fully automated production machine, 2 sides complete machining concept without turning station. Turning, drilling, milling, grinding and hard machining.
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
CNC vertical lathe with C axis indexing table and live spindle.
  • Hall: 17
  • Dalian Fullton Machinery Co., Ltd
The G 160 features a new concept for the high-productive grinding of gears up to 160 mm diameter with double work spindles, where separate X1 and X2 axes, driven by linear motors, replace the typical...
  • Hall: 26
  • Samputensili Machine Tools
The new 160HCD with Siemens SINUMERIK 840D sl CNC combines proven features with the innovative cutting chamfer technology for high quality gears with precise chamfers. Parallel to the gear hobbing p...
  • Hall: 26
  • Gleason Switzerland AG
The rigid construction bed are induction hardened over HRC50 and precision ground provides heavy duty turning and fine finishing at high accuracy. The main spindle is supported by selected and preloa...
  • Hall: 26
  • JESCO MACHINERY LTD.
The VTL-1600 Vertical Turning Center is a large, high precision, heavy duty machine, heavily ribbed for reduced thermal distortion and vibration dampening. Built for heavy duty turning of large size ...
  • Hall: 26
  • YOU JI MACHINE INDUSTRIAL CO., LTD
Fully electronic shaper head The new LS 180 E with electronic shaper head is characterized by superior flexibility. It can machine straight and oblique toothings in one clamping and can thus shap...
  • Hall: 26
  • Liebherr Verzahntechnik GmbH
Once again, GEMINIS will participate as exhibitor at the EMO 2019. In this edition, for the first time under the company name GEMINIS LATHES and with new corporate identity, GEMINIS will have a 20...
  • Hall: 26
  • GEMINIS LATHES
BOX GUIDE HORIZONTAL TURNING CENTER Stabilized structure that optimizing productivity. Product Features "Curvic" Coupling turret for easy maintenance after collision Rigid single tube type b...
  • Hall: 26
  • SMEC
AX200 MSY AX Series of machines, with live Y axis, are capable of performing several cutting processes such as turning, milling, drilling, tapping, deep-hole boring, etc. This series machines ...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
VMC 850nvu The series machine are much advanced and improved Gen - Next variant which is a new avatar of Vertical Machining Center satisfies the need of high speed, accuracy and reliability in per...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter