Search result

249 machines were found

2 axis (X, Z) SINUMERIK 840D sl, OP 010, MCP 483 PN
  • Hall: 11
  • TOS Hostivar s.r.o.
Matrix Machine Tool (Coventry) Ltd are pleased to introduce a true 5-Axis CNC, the Matrix M5C-0280 CNC Bevel Gear Cutting Machine suited to components up to 400 mm diameter, payload 100 kg and Module...
  • Hall: 11
  • Matrix Machine Tool (Coventry) Limited
5-axis universal machining center – pure technology in the smallest space Reduced machine width Fast tool change Tool loading on operator side Expandable tool pockets in the tool m...
  • Hall: 12
  • GROB-WERKE GmbH & Co. KG
Frame structure machining center by GROB Extra large work area, ideal for machining large frame structure parts such as subframes Unrestricted interference diameter of the A'-axis of 1,500 mm ...
  • Hall: 12
  • GROB-WERKE GmbH & Co. KG
G350 – Generation 2 with pallet changer system and robot cell Double pallet changer system compactly integrated into the machine Complete solution from a single source in a standardized desig...
  • Hall: 12
  • GROB-WERKE GmbH & Co. KG
The CorruGrind is used for producing corrugated rollers for manufacturing corrugated cardboard. Modern systems for corrugated cardboard operate with a paper run-through speed of up to 700 m/min. This...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
Horizontal Turning and Milling Center Complete machining with B-axis. B-axis and tool magazine add productivity to the VDF 450 TM for highly efficient manufacturing of small batches and medium vol...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Compact, fully automated production cell in cooperation with FFG Modul in Chemnitz followed by the gear cutting machine. Vertical machine concept with 2 x 12-fold tool turret arranged horizontally. ...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Horizontal Machining Center The single-spindle machine SPECHT 600 is widely configurable for use in flexible manufacturing systems. It is individually built in synchronised flow assembly for diverse...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Universal turning centers in the FFG portfolio offer a particularly wide range of applications and permit cost-effective use for single parts as well as small and medium batch sizes. A wide range of ...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
Vertical Power Skiving Machine for Gears and Shafts The integrated tool magazine enables additional operations like chamfering of the gears, turning, milling or drilling of holes. The machines are...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
High-Performance Vertical Milling Machine with linear Motor Technology
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
The single-spindle machine SPECHT 700 is widely configurable for use in flexible manufacturing systems. It is individually built in synchronised flow assembly for diverse loading concepts and a broad...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
The perfect balance between technology and compactness. We redesigned the working centre, to offer the best available technology, enriched with new and functional advantages. The new horizontal machi...
  • Hall: 17
  • Famar Srl
Four sizes TC300, TC400, TC600, TC800 Five turning lenghts 400 to 1,500 mm Tailstock or sub-spindle versions Siemens SINUMERIK 840D sl 24" touch-screen SPINNER I4.0 Panel Conversation...
  • Hall: 27
  • Spinner Werkzeugmaschinenfabrik GmbH
DX 200 NVU Renewed design with European aesthetics. Rigid bed and single piece 30 degree slant saddle. Rigid headstock spindle. High precision L.M. guide ways. Fast tool changing time just 0.5 s...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
The highly regarded VTC series has been installed in machine shops around the world for more than 20 years and the new VTC-530C and 760C are the latest additions to this successful range and are now ...
  • Hall: 27
  • Yamazaki Mazak
K3X8FIVE KX FIVE Series Machine is a high speed 5 axis machine suitable for all types of complex work pieces. The table is equipped with TRIM technology inclined at 55° plane allowing a tilting...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
VMC 1260nvu The series machine are much advanced and improved Gen - Next variant which is a new avatar of Vertical Machining Center satisfies the need of high speed, accuracy and reliability in ...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
The Umill 1500 machine have been perfectly designed for 5-axis machining operations such as milling, drilling, tapping and turning in one setup. Featuring a robust and rigid construction but yet prov...
  • Hall: 27
  • EMCO GmbH

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter