Search result

249 machines were found

Machine Description: SP425 is a 4 Spindle Single Pass Progressive Honing Machine with bore capacity of 5-15 mm and maximum bore length of 75 mm. It is developed specially for small components w...
  • Hall: 11
  • Khushbu Engineers
Another new product which Danobat will be showing at the trade fair is the VG-800 vertical grinding machine, which combines exterior and interior grinding and measuring operations for the manufacturi...
  • Hall: 11
  • DANOBAT S.Coop.
To cater for users who need the precision provided by grinding machines but do not wish to forsake the flexibility of turning machines, the firm is to present a high precision lathe LT-400 for turnin...
  • Hall: 11
  • DANOBAT S.Coop.
CNC Lathes from ROMI C Series are machines with great versatility for machining different types of parts, with great levels of power, quick movements and machining accuracy. With robust structure, hi...
  • Hall: 12
  • ROMI EUROPA GMBH
The vertical turning center is a portal construction. The 2 stands and cross-beams or truss form a closed framework, which ensures high rigidity and accuracy with the foundation . The possibili...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
Multiasking 5-axis vertical machining centre, trunnion table architecture and independent turning bar, for milling, turning and high-precision grinding operations. Engineered to provide its best effi...
  • Hall: 13
  • Breton Spa
The VCC 50 is based on the compact VCC series but is more stable and powerful than the basic model VCC. A powerful spindle and a particularly stable machine bed with a reinforced travelling column -...
  • Hall: 13
  • AXA Entwicklungs- und Maschinenbau GmbH
Horizontal machining center with dual spindle and pallet changer / system machine The SPECHT 500 DUO+ focuses on the market for components suppliers. It is based on a dual spindle model, successful...
  • Hall: 14
  • FFG Europe & Americas, MAG IAS GmbH
The ML200 is a horizontal deep hole drilling machine with 1, 2 or 4 spindles. The model is suitable for drilling injectors, inlet connectors, cooling channels in tools, smaller axles, sleeves, bone n...
  • Hall: 15
  • TBT Tiefbohrtechnik GmbH + CO
Handling of chuck parts up to 170 mm / 250 mm length and shaft parts up to 150 mm / 950 mm length in standard Fast creation of a process with predefined program modules Stacking of workpieces P...
  • Hall: 2
  • DMG MORI
RZ126 continuous generating gear grinding machine with integrated process monitoring. This machine features a twin spindle turret, which allows loading and meshing while one workpiece is being groun...
  • Hall: 26
  • Reishauer
The multiple award-winning thread rolling machine manufacturers EVIRT Italia with Nissei Co. Ltd. will present the RADIAL 50 Synchro Rolling Machine, which has been developed on the experience in rol...
  • Hall: 26
  • EVIRT ITALIA SRL
High-precision manual/CNC lathe combination made in Europe. Siemens CNC system: SINUMERIK 840D sl with Shop Turn (SINUMERIK ONE on fair model) Hydraulic chuck Automatic doors C-axes Driven...
  • Hall: 26
  • FAT Haco
Based on the well proven Genesis hobbing machines, the new 160HCD combines proven features with the innovative cutting chamfer technology for high quality gears with precise chamfers. Parallel to the...
  • Hall: 26
  • Gleason Sales
The rack grinding machine ZSM compact moves the machine table in the X direction (table machine). For helical racks, the grinding head slide to +/- 30° by manually pivoted. The basic machine includes...
  • Hall: 26
  • HABRAMA GmbH
The KNG 350 expert is based on a compact, set-up-optimised and modularized machine concept for use in medium and large-scale series production of externally geared components with a diameter of up to...
  • Hall: 26
  • KAPP GmbH & Co. KG
The UMILL 630 is the ideal universal milling center for 5-axis simultan-operation of parts with small or medium amount of production numbers, with a table size of 630 x 500 mm. The basic machine...
  • Hall: 27
  • EMCO GmbH
TACHYON 5 TACHYON 5 is a high speed drill-tap center, equipped with fast electro-mechanical type integral pallet changer, fast tool changer and a rapid of 60 m/min. This moving column drill tap ...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
TACHYON 7 TACHYON 7 is a high speed drill-tap center, equipped with fast electro-mechanical type integral pallet changer, fast tool changer and a rapid of 60 m/min. This moving column drill tap ...
  • Hall: 27
  • JYOTI CNC AUTOMATION LTD.
HELLER CNC ProfiTrainer. The training machine tool. The CNC ProfiTrainer is the heart of the HELLER learning factory. As a smaller counterpart of a large machine tool, the CNC ProfiTrainer of...
  • Hall: 9
  • Gebr. Heller Maschinenfabrik GmbH

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter