Search result

249 machines were found

The new range of APG-S centerless grinding machines is conceived with even higher possible integration into the manufacturing processes in conformity with Industry 4.0. It is efficient, performing an...
  • Hall: 11
  • RETTIFICATRICI GHIRINGHELLI SPA
The multi-technology center "millGrind" was specially developed for complex components and is available with 5 or 6 axes. It enables machining by grinding, milling and drilling (optional laser claddi...
  • Hall: 11
  • Elb-Schliff Werkzeugmaschinen GmbH
The compact MFP 30 5-axis grinding center from MÄGERLE is ideally suited for grinding complex geometries. The powerful drive of the high-performance spindle enables different grinding processes to be...
  • Hall: 11
  • MÄGERLE AG Maschinenfabrik
The Fill syncromill h21-63/500 machining center has been developed specifically for the machining of framework components, such as side members, crossmembers, and crossbeams from profiles or castings...
  • Hall: 12
  • Fill Gesellschaft m.b.H
HEDELIUS is presenting its Tiltenta 7-2600 at the EMO. It features x/y/z traverse paths of 2,600 x 750 x 695 mm and a pivotable main spindle. The 5-axis machining center has a 29 kW spindle which ope...
  • Hall: 12
  • HEDELIUS Maschinenfabrik GmbH
The new Direct Drive Rotary Table, integrated into machine bed, can rotate at high speeds for turning prismatic parts as big as Dia. 600 and also rotate at low RPM for milling applications. More ov...
  • Hall: 12
  • UCAM Private Limited
The C 42: a highly dynamic machining centre designed consistently for 5-axis/5-side machining. Features galore to ensure high-precision, economical parts production. Numerous automation solutions ext...
  • Hall: 12
  • Maschinenfabrik Berthold Hermle AG
The PowerTec is WALDRICH COBURG´s largest and most powerful portal machining centre. The modular design of this series lends itself to an extremely broad range of applications. As well as being avail...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
MasterTec is the portal machining centre for medium-sized, medium-weight workpieces with a module design. It can of course be adapted in various ways to suit all special requirements of our customers...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
The RailGrind is a high-precision grinding machine for manufacturing compact linear guideways. If the machine is equipped with two grinding supports, simultaneous grinding on both profile sides of th...
  • Hall: 13
  • Werkzeugmaschinenfabrik WALDRICH COBURG GmbH
The space within the machining zone has been maximized to prevent any tool interference and provide the utmost flexibility and substantically reduce any chance of collision between the cutting tools ...
  • Hall: 17
  • Focus CNC Co Ltd
The MIND-L 1000 was designed for hardening workpieces up to a diameter of 200 millimetres and a maximum length of 800 millimetres. The machine has X, Y and Z axes for positioning the inductors, one o...
  • Hall: 17
  • EMAG GmbH & Co. KG
Machine Features Powerful AC Spindle Motor High speed 4,000 rpm spindle Thermally stabilized spindle Linear motion guide ways 30 m/min rapid traverse rate Pre-tension ball screw support 0....
  • Hall: 17
  • ACE Designers Ltd.
Outstanding Performance of the New Era TTB-20 series make a limited space can be used with more flexibility. Excellent cutting performances with its compact floor space satisfy customers’ needs of...
  • Hall: 26
  • Taiwan Machine Tool Co. Ltd.
M30-G MILLTURN verfügt über einen Kuka-Roboter Kuka Robot KR Quantec extra sowie ein automatisches Greifertauschsystem mit zwei unterschiedlichen Greiferköpfen für Wellenkomponenten und Futterteile. ...
  • Hall: 26
  • WFL Millturn Technologies
High capacity, heavy duty, vertical boring & turning mills High quality cast iron constructions Full C axis and mill-spindle
  • Hall: 26
  • Hankook Machine Tools Co. Ltd.
In a world that constantly faces environmental challeges, Samputensili is proud to offer the SG 160 SkyGrind, the first gear dry grinding machine in the world. The machine is extremely environmental...
  • Hall: 26
  • Samputensili Machine Tools
The SH is a console machine (travelling column construction) and is distinguished by its compact and low-vibration design. The machine has an optional vertical axis with hydraulic weight compensat...
  • Hall: 26
  • SMS Maschinenbau GmbH
Vertical machining center with Siemens SINUMERIK 828D. Feed motors with 11 Nm for X/Y axis and 20 Nm for Z-axis. Spindle motor with 7 kW.
  • Hall: 27
  • Shandong Lu'nan Machine Tool Co., Ltd
The SPINNER VC1650-5A, which will be presented for the first time publicly at the EMO, is a 5-axis machining center for workpieces having a size of approx. 800 x 800 x 800 mm. One of the ...
  • Hall: 27
  • Spinner Werkzeugmaschinenfabrik GmbH

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter