Search result

249 machines were found

Along with these new machines, the firm's stand is to showcase a grinding machine made by its German subsidiary Danobat-Overbeck. The ILD-400, designed to grind interiors, exteriors and spokes and fo...
  • Hall: 11
  • DANOBAT S.Coop.
Along with these new machines, the firm's stand is to showcase a grinding machine made by its German subsidiary Danobat-Overbeck: the IRD-400, a fully automatic machine using a robot to load and unlo...
  • Hall: 11
  • DANOBAT S.Coop.
Die Schleifmaschine Vector Pendulum. Die Schleifscheibe schwingt zwischen zwei unabhängigen Spindelköpfen, von denen jeder für unterschiedliche Bedienschritte am selben Teil eingerichtet werden kann...
  • Hall: 11
  • Curtis Machine Tools Ltd
H 2000. Highly productive and reliable. Horizontal 4-axis machining centre with pallet changer as standard Top performance and short non-productive times for maximum productivity 2.8 sec. (spee...
  • Hall: 12
  • Gebr. Heller Maschinenfabrik GmbH
The new Direct Drive Rotary Table, integrated into machine bed, can rotate at high speeds for turning prismatic parts as big as Dia. 600 and also rotate at low RPM for milling applications. More over...
  • Hall: 12
  • UCAM Pvt. Ltd.
Robust well proved design, stable plate of the table for workpiece clamping Large clearance between the columns, small dimensions for building up High efficient drive of milling heads, torque on t...
  • Hall: 13
  • TOS KUŘIM - OS, a.s.
The ENDURA 700LINEAR is a state-of-the-art 5-axis milling machine in compact portal construction with linear motor drive technology and 5 CNC-controlled simultaneous axes. This machine tool is espe...
  • Hall: 13
  • Fooke GmbH
Small and compact, with a patented drive concept The RX10 is a compact processing centre with a very small footprint. Despite its compact appearance, the machine offers considerable processing ...
  • Hall: 13
  • Reiden Technik AG
High-precision 5-axis vertical machining centre with 2,000 x 2,500 x 800 mm travel, particularly suitable for hi-feed roughing, finishing and semi-finishing operations on medium applications on comp...
  • Hall: 13
  • Breton Spa
The ML270 is a horizontal deep hole drilling machine with 1, 2 or 4 spindles. The model is suitable especially for drilling gear shafts, VA-rails and other shaft-shaped workpieces, either manually lo...
  • Hall: 15
  • TBT Tiefbohrtechnik GmbH + CO
An improved turning center DZS 250/S is exhibited as a further developed product of the DZS series, which enables the machining of chuck components up to maximum swing diameter of 440 mm. The process...
  • Hall: 16
  • NSH Group
DMU eVo linear - The status quo in every industry The DMU eVo series combines the flexibility of high-tech universal milling machines and the performance potential of vertical machining centr...
  • Hall: 2
  • DECKEL MAHO Seebach GmbH
The EMCO MAXXTURN 45. The perfect solution for economic, off-the-shelf complete machining. Fitted with a counter spindle, driven tools, a high-precision C axis and extremely fast rapid motion speeds,...
  • Hall: 25
  • EMCO GmbH
The Atomat AT820E CNC is a versatile multi-functional integrated notching and marking machine. It is composed by the advanced notch milling machine, the sophisticated ROLLWORK software package, the...
  • Hall: 26
  • Atomat S.p.A.
The 260GX Threaded Wheel Grinding Machine is the latest addition to the highly successful Genesis series. The twin spindle concept combines maximum productivity with minimum idle and set up times...
  • Hall: 26
  • Gleason Sales
The 300PS Power Skiving Machine is well-suited for soft cutting and hard finishing of cylindrical internal and external gears. One of the highlights at the Gleason booth, the 300PS integrates a brand...
  • Hall: 26
  • Gleason Sales
Workpiece dimensions Swing over bed and slide - 820 mm Length (incl. 500 mm lg. face machining) - 3,000 mm Weight between chuck and tailstock with steadies - 8,000 kg Control Siemens S...
  • Hall: 26
  • Weingärtner Maschinenbau GmbH
The high-precision 5-axis CNC grinding machine 335linear is extremely flexible and universal. This flexibility allows you to meet all requirements for the production and resharpening of tools of all ...
  • Hall: 6
  • Alfred H. Schütte GmbH & Co. KG
The Multigrind CU . A big throw on 5.12 square meters. The long-awaited tool grinding machine from Haas. Perfect for high-precision ground cutting tools and smaller components. And anything but sta...
  • Hall: 6
  • Haas Schleifmaschinen GmbH
Multitasking 5-axis vertical machining centre, trunnion table architecture and independent turning bar, for milling, turning and high-precision grinding operations. Engineered to provide its best eff...
  • Hall: 9
  • Breton Spa

Company

FFG Europe & Americas, MAG IAS GmbH 16 Werkzeugmaschinenfabrik WALDRICH COBURG GmbH 12 DMG MORI 9 JYOTI CNC AUTOMATION LTD. 9 GROB-WERKE GmbH & Co. KG 8 DANOBAT S.Coop. 7 EMAG GmbH & Co. KG 6 EMCO GmbH 5 Gebr. Heller Maschinenfabrik GmbH 4 Liebherr Verzahntechnik GmbH 4 Gleason Sales 4 DECKEL MAHO Seebach GmbH 4 UNISIGN Machine Tools 4 Starrag AG 3 CHIRON Werke GmbH & Co.KG 3 Fill Gesellschaft m.b.H 3 Matrix Machine Tool (Coventry) Limited 3 Breton Spa 3 SMEC 3 Hanwha Precision Machinery Co., Ltd 3 Hyundai Wia Corporation 3 DOOSAN MACHINE TOOLS 3 Haas Schleifmaschinen GmbH 3 WFL Millturn Technologies 3 TONGTAI MACHINE & TOOL CO., LTD. 2 Spinner Werkzeugmaschinenfabrik GmbH 2 TBT Tiefbohrtechnik GmbH + CO 2 Priminer machine tools Dongguan Co.,ltd 2 Schwäbische Werkzeugmaschinen GmbH 2 Yamazaki Mazak 2 Atomat S.p.A. 2 SMS Maschinenbau GmbH 2 Samputensili Machine Tools 2 Famar Srl 2 Hüller-Hille 2 XYZ Machine Tools Ltd 2 Reiden Technik AG 2 INDEX-Werke GmbH & Co. KG 2 Alfred H. Schütte GmbH & Co. KG 2 HABRAMA GmbH 2 Curtis Machine Tools Ltd 2 ŠKODA MACHINE TOOL a.s. 2 KAPP GmbH & Co. KG 2 YOU JI MACHINE INDUSTRIAL CO., LTD 2 NSH Group 2 Taiwan Machine Tool Co. Ltd. 2 Guangdong Hotman Intelligent Machine Co.,Ltd 2 Jobs SpA 1 Gioria s.p.a. 1 RETTIFICATRICI GHIRINGHELLI SPA 1 F. Zimmermann GmbH 1 J.G.WEISSER SÖHNE 1 HURON GRAFFENSTADEN 1 Reishauer 1 ACE Designers Ltd. 1 UCAM Private Limited 1 Carl Benzinger GmbH 1 AXA Entwicklungs- und Maschinenbau GmbH 1 LEADWELL CNC MACHINES MFG., CORP. 1 Loch Präzisionsbohrtechnik GmbH 1 ELHA-MASCHINENBAU Liemke KG 1 TOS Hostivar s.r.o. 1 DMT Drehmaschinen GmbH & Co. KG 1 Matrix Machine Tool (Coventry) Limited 1 Maschinenfabrik Berthold Hermle AG 1 ROMI EUROPA GMBH 1 zayer 1 Erwin Junker Maschinenfabrik GmbH 1 Mikron Machining 1 MÄGERLE AG Maschinenfabrik 1 Kunzmann Maschinenbau GmbH 1 BELOTTI S.p.a 1 Weingärtner Maschinenbau GmbH 1 C.B. FERRARI 1 ALZMETALL GmbH & Co. KG 1 Fooke GmbH 1 BURKHARDT+WEBER Fertigungssysteme GmbH 1 Dalian Fullton Machinery Co., Ltd 1 MABI Robotic AG 1 R&D Maschinenbau GmbH & Co. KG 1 EVIRT ITALIA SRL 1 Willi Seiger GmbH 1 FAT Haco 1 TOS KUŘIM - OS, a.s. 1 PAMA 1 Shandong Weida Heavy Industries Co.,Ltd 1 Shandong Yourong Machine Tool Co., Ltd. 1 Shandong Lu'nan Machine Tool Co., Ltd 1 Khushbu Engineers 1 ROBBI Group S.r.l. 1 PING JENG MACHINERY INDUSTRY CO., LTD. 1 O.M.V. Officine Meccaniche Venete S.p.A. 1 Mandelli Sistemi Spa 1 TOSHULIN, a.s. 1 Felsomat GmbH & Co. KG 1 MCM SpA 1 HEDELIUS Maschinenfabrik GmbH 1 Elb-Schliff Werkzeugmaschinen GmbH 1 Komatech 1 HWACHEON Machine Tools Co., Ltd 1 Hankook Machine Tools Co. Ltd. 1 Yeong Chin Machinery Industries Co. Ltd. 1 Mikromat GmbH 1 UCAM Pvt. Ltd. 1 YUYAO BUMBLEBEE TECHNOLOGY CO.LTD 1 SAMAG Saalfelder Werkzeugmaschinen GmbH 1 Yiteli (Shanghai) Technology Co., Ltd. 1 Manford Machinery Co., LTD. 1 Fair Friend Ent.CO., LTD. 1 SUN FIRM MACHINERY INDUSTRIAL CO., LTD. 1 Starrag AG 1 Nanjing Ningqing CNC Machine Tool Manufacture Co.,Ltd 1 Gleason-Pfauter Maschinenfabrik GmbH 1 Gleason Switzerland AG 1 Niles-Simmons-Hegenscheidt GmbH 1 Imoberdorf AG 1 BEAM MACHINES 1 STAMA Maschinenfabrik GmbH 1 GEMINIS LATHES 1 Focus CNC Co Ltd 1 JESCO MACHINERY LTD. 1 Shenzhen Create Century Machinery Co., Ltd 1 Guangzhou Minjia Manufacture Technology Co. Ltd. 1 Foshan Pratic CNC Science & Technology Co., Ltd. 1 E. Zoller GmbH & Co. KG 1
Load more...

Languages

Reminder lists

Filter