11/7/2011 2:15 PM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear smiffy, If I understand it correct, the intent of the code is to copy 76 bytes from the BYTE-offsets x * 78 to the BYTE-offset 780. The ANY-pointer contains in Byte 7-9 the BIT-offset of the adress, so I think it's correct to multiply the BYTE-offset with 8 to get the BIT-offset. The format of the ANY-datatype is described in A.3.4.5 of the manual Best regards, yy1 |
Follow us on