6/11/2011 9:57 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Perhaps if your PG is "old" version (means with Windows XP) this FAQ could helps What remedies are possible if you cannot shut down your computer in Windows XP mode? Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/11/2011 10:01 AM | |
Posts: 2964 Rating: (478) |
Hello Umencho, I have checked this.....completely but it is not helping in my way....by any chance do you have Bios veriosn of 14.01.03.... Regards, Ekalavya |
6/11/2011 10:10 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Siemens update bios for M3 http://support.automation.siemens.com/WW/view/en/48791866 Why does people want to play with BIOS update so often? Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 6/11/2011 10:11 AMtypo |
|
This contribution was helpful to1 thankful Users |
6/11/2011 10:54 AM | |
Posts: 8946 Rating: (999) |
This link do not have a possibility to do a download. You have to contact the support! |
6/11/2011 1:47 PM | |
Posts: 947 Rating: (45) |
Hi EKALAVYA see: http://support.microsoft.com/kb/313290/en-us. May be should reinstall chipset driver and setting CPU driver (see attach) Attachment3.ZIP (559 Downloads) |
This contribution was helpful to1 thankful Users |
6/12/2011 11:32 AM | |
Posts: 947 Rating: (45) |
Hi EKALAVYA Your problem is likely due to ACPI, may set the wrong driver CPU. Check it out. (see attach above) Is there a problem when running without battery? If this fails, then you need to update the BIOS. If you have a problem with loading the BIOS, can I download the update file to file sharing, such Filesonic |
This contribution was helpful to1 thankful Users |
Follow us on