5/29/2010 8:04 AM | |
Posts: 163 Rating: (0) |
Dear all, |
5/29/2010 8:11 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Use the same logic. This manual will helps you - WinCC: Working with WinCC best regards, Hristo Mihalev |
5/29/2010 8:49 AM | |
Posts: 63 Rating: (39) |
Dear Sindhu, U can easily do this using c script see the attachment copy the function "Word_bits" in Library of your project folder then open the C-Editor in wincc explorer, generate header in it close c-editor and save it, if ask then open the button properties in graphics designer creat a c-action on mouse click event open the project function and double click the "word_bits" then attach a tag in the tag field and in bit No write "0(Zero)" then press ok activate project and see the action If helpful then RATE me From Mack AttachmentSc.zip (1135 Downloads) |
Last edited by: mack123 at: 5/29/2010 8:53 AM |
|
This contribution was helpful to2 thankful Users |
5/29/2010 8:50 AM | |
Posts: 163 Rating: (0) |
I have that manual....detailed step is not found for inverting the bit.can you give a me step by step process |
5/29/2010 8:52 AM | |
Posts: 163 Rating: (0) |
Mack, let me trythe steps and come back to you |
5/29/2010 8:58 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi Sindhu, Please Checked this postI have posted the C Script for the Same. |
Ammy |
|
5/29/2010 11:05 AM | |
Posts: 163 Rating: (0) |
The file asks for a password |
Follow us on