3/25/2024 6:46 AM | |
Joined: 3/11/2019 Last visit: 5/8/2024 Posts: 1408 Rating: (255) |
Hi
unclear is this part. Because there are indeed dependencies that f-inputs can not be shown in watch tabels and in the "standard" user program. But in F-program, it must work. So are you sure the input/channel is really used in the f-program and is this program also downloaded to the cpu? Why does the status of fail-safe inputs and outputs not change in the watch (monitoring) table?regards sancruz |
Feedback appreciated, please rate |
|