10/19/2014 12:12 PM | |
Posts: 6 Rating: (0) |
IS there is Any manuals for the following devices NCRS NICO NRK16 B/A NABBS Except Integral AS1000 Thanks |
10/23/2014 11:47 AM | |
Posts: 6 Rating: (0) |
Albis Thanks for your reply i can request the programming and communication softwares ? Best regards Ahmed |
10/23/2014 3:29 PM | |
Posts: 6 Rating: (0) |
Dear Albis Does the migration require to replace the NRK16, NCRS, anD the other devices with new Devices Really apreciate your replays Thanks Best Regards Ahmed |
10/24/2014 9:06 AM | |
Joined: 6/4/2010 Last visit: 6/5/2024 Posts: 379 Rating: (127) |
Dear Ahmed,
Depending on the exact situation, you can replace the management level only, the whole automation level or the automation and the field devices. The best migration strategy depends on the age of the installation, the future plans for the building(s) and on your specific requirements. I recommend to exchange the management level (NCRS) and automation level (NRK16 etc.) together normally, if the installation is more than 15 years old. You may split the migration work and start with one panel. Your local Siemens BT office can help you with the best possible migration strategy for your system. Best regards, Albis |
6/23/2016 1:45 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Danistocks is split to a separate thread with the subject How to reboot/reset the AS1000 integral without affecting the settings already set?. Best regards |
Follow us on