4/23/2024 2:14 PM | |
Joined: 10/18/2023 Last visit: 5/8/2024 Posts: 2 Rating: (0) |
Hello All , I just trying to send CW and CLK signal to step motor driver with 6ES7 138-6DB00-0BB1 . I made configration as a pulse output on hardware config. And using the LPD library to control unit. I tried everything it wasnt worked. I made a lot of research there arent anything execpt one valve control example but it wont help me. Due to my cpu i could not config the positioning axis 4.0 ( I'am using the 1516-3 pn/dp) Have a great day all! Attachmentproblem.zip (4 Downloads) |
4/24/2024 1:05 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, S7-1516 supports TO's. Choose the possible version. The configuration is described in the manual. 5.2.6 Connecting stepper motors (S7-1500, S7-1500T) Drives with a stepper motor interface are connected using telegram 3 and with the help of PTO (Pulse Train Output) pulse generators. Use the following modules to control the stepper motors: • TM PTO 2x24V / TM PTO 4 https://support.industry.siemens.com/cs/ww/en/view/109817884 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
5/2/2024 3:21 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, 6.4.4 TM Pulse 2x24V (S7-1500, S7-1500T) For use with Motion Control, the parameters described below must each be configured: Drive connection using PWM (pulse width modulation) https://support.industry.siemens.com/cs/ww/en/view/109817883 |
With best regards, |
|
Follow us on