4/17/2024 11:38 AM | |
Joined: 1/21/2013 Last visit: 5/6/2024 Posts: 2743 Rating: (444)
|
Hi Artur1957842, Could you please let us know which product you are talking about? Kind regards |
4/17/2024 12:22 PM | |
Joined: 1/4/2021 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Thank You for answer I work with S-1500 1515-2 PN PLC |
4/18/2024 11:07 AM | |
Joined: 8/3/2009 Last visit: 5/6/2024 Posts: 12882 Rating: (1645) |
Hello Artur1957842 In this FAQ there are also a few information about getting access to the Datalogs or to send them https://support.industry.siemens.com/cs/de/en/view/64396156 bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
4/22/2024 7:57 AM | |
Joined: 1/4/2021 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Hi Murof Yes, I saw and read this article, but I would not like to use the TMAIL_C function because it defeats my purpose, which is direct writing to FTP.I'm still thinking about using the FTP_CLient/Server or FTP1X00CMD functions.What do you think about this solution? |
4/23/2024 8:47 PM | |
Joined: 1/19/2018 Last visit: 4/29/2024 Posts: 2 Rating: (0) |
If I understand clearly, your goal is to log any data and do a daily transfer on FTP server (simply: backup this datalogs somewhere in cheap and simply way) I have now same problem and I have found same solutions. In my opinion, don't use SD card for saving big data repeatedly. Simatic SD is not cheap stuff... I want to use FTP server on RPi or NanoPi. FTPserver based on vsftpd (there is lot of manuals for setup). During day you will log data in DB and then, using LFTP library, you save this data in correct way where you need. Other good solution is useConPLC by marvin-mangold, but it depends on your application. |
Last edited by: topmartin at: 04/23/2024 21:00:37MS SQL Last edited by: Jen_Moderator at: 04/24/2024 08:47:44Text formatting optimized. |
|
4/24/2024 1:14 PM | |
Joined: 8/3/2009 Last visit: 5/6/2024 Posts: 12882 Rating: (1645) |
Hello Artur1957842 perhaps this way could give a possibility to send data to FTP: https://support.industry.siemens.com/cs/de/en/view/103550797 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on