4/18/2024 10:21 AM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
I have a problem an analog problem too I'am reading the analog output of a Siemens Micromaster 420 whish is 0mA to 20mA using "picture 1" and sending speed using "picture 2" and i made a simple HMI. Everything is fine however in the BACKWARD rotation i can't read the 0% to -100% speed cause of course the drive's output doesn't provide 0mA to -20mA, that i understand Is there a way by either logic, magic or the power of will that allows to invert the "speed reading in percent"(%MD8) value so i can read the -0% to -100% speed ? Sorry, couldn't add multiple attachments he he ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_5311751 at: 04/18/2024 10:22:36Last edited by: AutoGen_5311751 at: 04/18/2024 10:24:46Last edited by: The Helping Hand at: 04/18/2024 13:45:35New subject after splitting Professional Noob :p |
|
4/18/2024 10:29 AM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
|
Professional Noob :p |
|
4/18/2024 10:30 AM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
|
Professional Noob :p |
|
4/18/2024 2:19 PM | |
Joined: 9/23/2005 Last visit: 4/30/2024 Posts: 4524 Rating: (698)
|
A little bit of magic is required. Change speed scaling in the Micromaster, so 0 mA = -100%, 20 mA = 100%. Adjust the PLC code accordingly. |
Regards, |
|
4/21/2024 1:36 PM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
First of all !!! I want to thank you for your time and response Second, i suppose P1 is where i can....."play". continue to pictures 4 and 5 |
Professional Noob :p |
|
4/21/2024 1:39 PM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
|
Professional Noob :p |
|
4/21/2024 1:42 PM | |
Joined: 1/2/2024 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
It seems that Siemens doesn't believe in magic but only in bytes and bits |
Professional Noob :p |
|
Follow us on