3/14/2023 11:57 AM | |
Joined: 8/12/2021 Last visit: 6/4/2024 Posts: 309 Rating: (29) |
Hi! Maybe you can check with a hard disk analysis tool to see if there is a problem detected in any sector (it is possible that it has been damaged). Another test I can think of, is to try, when you boot and this error appears, boot again and access the BIOS to see if the hard drive is recognised. Also check the BIOS version here and if it is old, you might want to consider upgrading. |
If this Information really helps, you could use the Rate function |
|
Follow us on