1/3/2024 9:11 AM | |
Joined: 7/27/2023 Last visit: 5/10/2024 Posts: 46 Rating: (4) |
Hi! In response to the second question, about the max memory, as you explained in PG M5 release note, RAM can be expanded up to 32GB. However, in the case of its successor, PG M6, RAM can be expanded up to 64GB. - Delivery release for SIMATIC Field PG M5: https://support.industry.siemens.com/cs/es/en/view/109737135 - Delivery release SIMATIC Field PG M6, Edition 2023, with TIA Portal V18: https://support.industry.siemens.com/cs/es/en/view/109817602 |
Last edited by: The Helping Hand at: 01/03/2024 13:20:55Text fomatting and links optimized |
|
1/6/2024 3:59 AM | |
Joined: 8/28/2018 Last visit: 5/9/2024 Posts: 2 Rating: (0) |
Thank you for the information, And today I found the shutdown problem more intreseting, as I turn on my BT mouse the system comes with the noticfacation sound and suddenlly freezed (sound remains one tone) then after 1~2 seconds system reboot itself, so the issue might be related to hardware recognition not the memory. but I'm not sure if the cause is the same (dosen't boot up / suddenlly shutdown) Or it still might be caused by the bad battery, because I plug the cord and turn on my mouse just after 1 second. New battery still not recived, I'll update if the problem solved. Thanks Dean |
Follow us on