3/8/2023 2:02 PM | |
Joined: 11/19/2016 Last visit: 4/8/2024 Posts: 35 Rating: (0) |
Hi, I am facing one issue in S7-412-5H system. During operation all CPU LED's turned off. and after power restart all LED's started flashing. After powering restart by putting CPU in stop mode it started normally but the program got erased from the CPU. the diagnostic buffer we have saved from CPU is attached. In that we observed that error description was mentioned as "Memory reset due to Inconsistent data" . Can anyone help us in understanding the possibilities of the error occurence ? Can this happen because of hardware issue? AttachmentDiagnose.txt (503 Downloads) |
Follow us on