9/13/2013 5:02 PM | |
Posts: 510 Rating: (117)
|
If your 505 CPU has a Profibus Connector you can use the DP DPcoupler. You can transfer 244 bytes perPLC scan. billwest |
9/14/2013 10:59 AM | |
Posts: 19 Rating: (0) |
Addition Configuration of used . (Config V2.0) Please see attachement file and advice is correct or not? Regards, Alex. |
9/16/2013 4:15 PM | |
Posts: 510 Rating: (117)
|
I have attached the IE/PB manual. In reviewing the manual, it doesn't preclude connecting a 505 CPU with the ISO protthe CPU to stopocol. I just don't see a mechanism for getting or putting data from the 505 on the S7300 through Profibus without making changes to the S7-300 program. The S7-300 program can be modified without stopping the CPU. Hardware changes require. I don't know where to go from here. billwest
AttachmentIePbLink_e.pdf (645 Downloads) |
Follow us on