5/10/2023 6:02 AM | |
Joined: 1/21/2013 Last visit: 5/14/2024 Posts: 2775 Rating: (448)
|
Hi, I have made some attempts myself to configure VLAN for devices in the same project. It seems that it's only possible to compile if the switch is not connected to a subnet. So I created a configuration where the switch was not connected in the network view, but active port connections in the topology view. This configuration compiled without errors. However, since I wasn't able to test it on hardware, I can't really say if this will work or if this is the recommended configuration. I recommend that you contact technical support and create a support request. And please do us a favor and post the answer they give you. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on