2/5/2022 12:35 AM | |
Joined: 7/14/2021 Last visit: 2/5/2022 Posts: 1 Rating: (0) |
Estimated: Estimated: I need to communicate with a PLC Siemens, S71200 in V15.1 Tia Portal Version, and the software required the file: gsdml-v2.32-tr-0153-pnrotative2-20180518.xml 1.0SD This file is of Encoder TR ELectronic, I browsed in the manual, and I don't found this file. Can you send me this file ?? Thanks and regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/07/2022 06:32:11New subject after splitting |
|
2/5/2022 4:52 AM | |
Joined: 12/18/2014 Last visit: 5/14/2024 Posts: 33032 Rating: (4082) |
Hello Lisalfonzo, is your google broken? I search 2 minutes and then I found it. File download: tr-electronic.de then in the section Industrial EthernetThe XML file (device description file) contain all information about the measuring system-specific parameters and the measuring system’s operating modes. The XML file is integrated using the network configuration tool to correctly configure or operate the measuring system and is included in the package contents. The zip file contains device description for: PROFINET, PROFINET/Profisafe, Ethernet/IP, EtherCAT, Powerlink, SercosThere you can download the zip file. Your files are in the folder: TR-ECE-ID-MUL-0055-09\previous version. AttachmentTR-ECE-ID-MUL-0055-09.zip (175 Downloads) |
This contribution was helpful to2 thankful Users |
4/28/2024 11:31 AM | |
Joined: 12/18/2014 Last visit: 5/14/2024 Posts: 33032 Rating: (4082) |
Contact the manufacturer ... |
This contribution was helpful to1 thankful Users |
Follow us on