2/17/2017 7:18 AM | |
Posts: 1 Rating: (0) |
Hi, I want to use SIRIUS SAFETY RELAY STD RELAYS 3NO+1NC 3SK1111-1AB30 Operating current at 17 V minimum = 5mA where as Control supply voltage at DC = 24VDC with Operating range factor at DC = 0.85 to 1.2 24DC at 8.5% = 20.4VDC, then Operating Current given for 17V = 5mA. can any one please explain why it is given for 17V where as Min Operating range = 20.4VDC? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/17/2017 12:22:55 PMNew subject after splitting |
|
2/17/2017 1:49 PM | |||
Posts: 467 Rating: (59)
|
hello, Operating range factor control supply voltage rated value of magnet coil 0,85..1,1 is for the powersupply A1/A2
|
||
1/4/2024 1:26 PM | |
Joined: 6/19/2017 Last visit: 5/29/2024 Posts: 8119 Rating: (165) |
New question published by DAM54 is split to a separate thread with the subject SIRIUS SAFETY RELAY: Whats the current at 24VDC of this coil? . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on