4/4/2024 5:59 AM | |
Joined: 3/11/2019 Last visit: 5/15/2024 Posts: 1414 Rating: (255) |
Hi, perform the memory reset as requsested in the error message. How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)?You can try this first: MMC All the user data is deleted when you reset the SIMATIC Micro Memory Card (MMC). Proceed as follows.
If the CPU continues to request an overall reset after the procedure described above, then the MMC is defective. regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on