3/24/2024 9:39 AM | |
Joined: 2/28/2023 Last visit: 5/15/2024 Posts: 38 Rating: (1) |
Mate. Measuring data with a PLC and and recording on PC requires a PC/PLC connection provided through TPC/IP protocols which an Ethernet cable cat6 can provide. Python programming provides data extraction from PLC to PC using a specific python library (python-snap7). Siemens LOGO! series support TCP/IP communication protocol and also other PLC like S7-1200 which you are using the only variable are the protocols and python script Further information on PLC/PC communication are provided here S7 Communication between S7 CPU and PC station (siemens.com) ------------------------------------------------------------------------------------------------------Is it resourceful? Ooh Really. Why not rate if you wish |
Cheers. |
|
3/25/2024 2:53 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2370)
|
Look for a Siemens FTP type library component. Check this link for a good starting point: https://support.industry.siemens.com/cs/document/109780503
|
science guy |
|
3/25/2024 3:03 PM | |
Joined: 3/22/2024 Last visit: 5/1/2024 Posts: 7 Rating: (0) |
Thank you ! |
Follow us on