11/14/2022 10:38 AM | |
Joined: 7/5/2022 Last visit: 5/17/2024 Posts: 9 Rating: (0) |
Hi Is it possible to upload backup of CPU 551 installed on rack 5213 with CP50M1 and CP51M1. |
11/14/2022 10:45 AM | |
Joined: 8/25/2006 Last visit: 6/7/2024 Posts: 2206 Rating: (278)
|
Hello. Uploading from Simatic TDC is not possible. |
This contribution was helpful to1 thankful Users |
12/8/2022 5:51 AM | |
Joined: 7/5/2022 Last visit: 5/17/2024 Posts: 9 Rating: (0) |
Hi, DUST 1 communication protocol in not installing by add/remove option in PG PC settings. what should do? |
12/8/2022 7:45 AM | |
Joined: 8/25/2006 Last visit: 6/7/2024 Posts: 2206 Rating: (278)
|
According to D7-SYS-Readme (chapter 9.24) I think you need at least HF3 or higher for D7-SYS V6.2 SP3, ask Siemens for it, as it is not available for download. |
Follow us on