10/9/2018 11:40 AM | |
Posts: 8 Rating: (0) |
Hello Evereyone I am having one masibus 85xx+ scanner. I want the plc (s7 1200 cpu1214c) to read temperature values. I have used MB Client instruction in programme but showing error 7006. The scanner communicates via modbus TCP/IP interface. I am enclosing a zip file containing pic of scanner settings and the v13 programme that i have made. Pls help, its urgent Thanks AttachmentMODBUS TCP TEST 1.zip (998 Downloads) |