9/26/2008 12:39 PM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating: (26) |
Hi JMJ, That answer is exactly what I need . I will inform you after I try Regards |
Genetic Fuzzy PID Controller |
|
9/27/2008 1:36 PM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating: (26) |
Hi JMJ, I still have problem with Sentron, Best regards, |
Genetic Fuzzy PID Controller |
|
9/29/2008 2:28 PM | |
Posts: 487 Rating: (44) |
I think it because your DP data is with "Total Consistancy". You have two options here.
So the parameters for SFC will look like. |
1/7/2009 4:36 PM | |
Joined: 1/7/2009 Last visit: 3/27/2024 Posts: 25 Rating: (0) |
Hello: I have a Pac3200 networked. I am trying to connect 7 WinCC Modbus TCP-IP, and not me. However communicates perfectly with powerconfig. I do not place any more in such settings. |
1/7/2009 11:18 PM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating: (26) |
Hello Oscar, Do You meant to say that you connect and read the variables with wincc7 ? I try to connect with simatic step7, and as JMJ said , i tried as PID256 or whatever I want to read I could be able to read the variables, but I havent tried with wincc7, its good to learn if you will explain. best regards |
Genetic Fuzzy PID Controller |
|
1/8/2009 9:36 AM | |||||
Joined: 1/7/2009 Last visit: 3/27/2024 Posts: 25 Rating: (0) |
|
||||
1/8/2009 2:03 PM | |
Posts: 487 Rating: (44) |
You do notneed to add any new hardware on WinCC. WinCC7.0 has ModbusTCP/IP channel DLL available. So you can add this channel and configure connection using the ethernet card of your PC. It is also possible to use any third party OPC server softwarefor Modbus TCP to communicate to WinCC. Please check the attached manual for Modbus TCPIP channel driver manualfor WinCC 7.0 AttachmentModbusTCPIP.pdf (860 Downloads) |
Last edited by: JMJ at: 1/8/2009 2:10 PM |
|
3/28/2009 12:13 AM | |
Joined: 5/17/2006 Last visit: 2/26/2024 Posts: 218 Rating: (26) |
Thank you very much for your help, In order to read data, its better to insert seperately one by one. as JMJ 's example , current L1 - current L2 - current L3. Also I dont use universal - because then I need to extract values again. Best regards, |
Genetic Fuzzy PID Controller |
|
10/15/2009 8:42 AM | |
Posts: 133 Rating: (9) |
Hi Candy I figured that the hard way. I am configuring a basic type 2. But when I use the Basic Type 2 I do not read any values from the device. It works if I add the Voltage a-b, Voltage b-c, Voltage a-c separately. I do not receive values for the Active Energy Inport Tariff 1 (D). Now that I am reading the values into the PLC. I am struggling to use the existing Block icons and Faceplates to intergrate into WinCC. I have read the manuals that are provided with SIMATIC WINCC Powerrate. DOes anyone know how to intergrate these blocks to the block icons and faceplates? |
5/7/2015 4:55 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|