8/7/2023 7:03 AM | |
Joined: 2/10/2015 Last visit: 4/29/2024 Posts: 95 Rating: (11) |
Hi, depending on how the reader is configured, you first need to send a command to the reader using the write command. That has to be done if default settings are used. The commands can be found in the manual, in the section describing serial communication. Here's a application axample. The reader can also be configured to use unidirectional communication mode. E.g. if you're only interested in the UID. Then your approach can be used, but then you can't send commands to the reader. |
This contribution was helpful to1 thankful Users |