5/12/2006 9:24 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi, Perhaps the following link will help you, http://support.automation.siemens.com/WW/view/en/19449428 It's a master - slave configuration, unfortunaly the S7-400 is master and S7-300 is slave. But I hope it will help you, Wizard |
5/18/2006 3:59 PM | |
Posts: 22 Rating: (0) |
Hi All AttachmentBel1.zip (616 Downloads) |
5/18/2006 4:21 PM | |
Posts: 22 Rating: (0) |
Hi All how can i do hardware configration? how can l perform configuratelikeattached folder and how can ı use sfc14-sfc15. For example ı want to read analog output from slave plc and i wantto write any data block to master plc. Attachment46.zip (688 Downloads) |
5/18/2006 4:45 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi, The following link is a manual where SFC14 and SFC15 are explained: http://support.automation.siemens.com/WW/view/en/1214574 In the configuration tab of the S7-318 (slave), you can specify how many byte's or words you want to communicate. Greetings, Wizard |
5/22/2006 9:52 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi erenakc, When you want to use PUT and GET, you'll have to use FB14 and FB15 in the S7-300. And you'll have to use a CP342-5. See the following link: http://support.automation.siemens.com/WW/view/en/22991863 But with the hardware you've got, you can use SFC14 and SFC15, see the attachment project. Best regards, Wizard Attachmenttest.zip (569 Downloads) |
5/31/2006 1:10 PM | |
Posts: 22 Rating: (0) |
Thank you for solitions.İf it is possible can you send simple project about dp send and dp receive Best regard |
5/31/2006 2:03 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello erenakc Good luck with sample project. Greetings Wizard Attachmenttest1.zip (451 Downloads) |
5/31/2006 6:29 PM | |
Posts: 22 Rating: (0) |
hi Friend Can you say or send document,which functions where can ı use.Example x-get and x-put functions i use with mpı protocol Thanks |
6/1/2006 9:51 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hi erenakc, I hope the following links will help you. http://support.automation.siemens.com/WW/view/en/21537047 http://support.automation.siemens.com/WW/view/en/20982954 http://support.automation.siemens.com/WW/view/en/6990694 Unfortunaly I don't have an example with X-put. The following manual will explain the functions X-put and X-get http://support.automation.siemens.com/WW/view/en/1214574 Greetings, Wizard |
Last edited by: Wizard at: 6/1/2006 9:54 AM |
|
Follow us on