7/29/2013 2:47 PM | |
Posts: 5 Rating: (15) |
To install STEP 7 v5.5 SP3 (DVD update release) follow these steps. 1. Download and install the latest 64-bit version of automation licence manager. http://support.automation.siemens.com/WW/view/en/114358 2. Copy DVD content to any directory on hdd. 3. Modify ./Setup.exe using any resouce modification software. Eg ResourceHack. Add the line <supportedOS Id="{4a2f28e3-53b9-4441-ba9c-d69d4a4a6e38}"></supportedOS> //this is the os ID of Windows 8 64bit 4. Modify ./InstData/Setup.ini under section OS. PlattformIDAllowed = 1;2;3 Add the lines Win8x64=1 5. Modify all msi-files to enable the ingore-button on installation failures (like installing on unsupported OS's). Use any software possible to manipulate MSI-files. E.g. InstEd. Search for DLG_INSTALLATIONREQUIREMENTS_DISABLE_IGNORE. Change Action from Disbale to Enable. Run ./Setup to start installation. Press the ingore-button when told it's not possible to install on running OS.Good luck! Disclaimer. I can not be held responsible to any result caused by following this guide. It's just for educational purposes. |
This contribution was helpful to21 thankful Users |
9/6/2013 11:48 AM | |
Joined: 9/11/2011 Last visit: 5/6/2024 Posts: 52 Rating: (0) |
Thanks friend |
1/5/2014 11:56 AM | |
Joined: 1/28/2009 Last visit: 1/22/2022 Posts: 21 Rating: (0) |
Dear sir I need more explanation. because i can't follow your method and i still can't install it thanking you |
3/21/2014 12:42 PM | |
Posts: 1 Rating: (0) |
hello i'm be so happy if you learn us with picture to how do this rule you said in this post. tnx |
4/7/2014 10:01 PM | |
Joined: 1/12/2010 Last visit: 12/18/2023 Posts: 5 Rating: (0) |
can you give us more explaination with photo |
4/12/2014 12:48 PM | |
Posts: 1 Rating: (0) |
you can not tell me more? if any pictures are great too! thank you! performed in step 4 how so?
|
6/23/2014 10:30 PM | |
Posts: 4 Rating: (0) |
I just recieved the same error. I am attempting to uninstall and re-install Step 7 ... crossing my fingers. |
6/30/2014 4:37 PM | |
Posts: 2 Rating: (0) |
I didn't understand where I should add these lines. Can you please,explain more with some screen shots ? |
6/30/2014 4:38 PM | |
Posts: 2 Rating: (0) |
I didn't understand where I should add these lines. Can you please,explain more with some screen shots ? |
9/23/2014 9:05 AM | |
Posts: 1 Rating: (0) |
Dear JonasBentsson, Can you guide step by step? I'm using Windows 8.1, I use Resource Hacker software but I don't known "add the line support windows 8.1" and modify msi files. Thanks.
|
Last edited by: WhiteTiger at: 9/23/2014 9:06 AM |
|
10/20/2014 10:59 AM | |
Joined: 1/28/2013 Last visit: 4/22/2024 Posts: 37 Rating: (8) |
Brother its not working i cant installing on windows 8.1 can you help me..? |
10/23/2014 4:11 AM | |
Posts: 2 Rating: (3) |
Successful in windows 8.1 64bit. I'm using Step 7 v5.5 SP4. Thanks for guide!
|
10/26/2014 12:29 AM | |
Posts: 4 Rating: (0) |
Brothers Help me please |
10/27/2014 2:58 AM | |
Posts: 2 Rating: (3) |
Dearراغب: You must install Step 7 before install Step 7 v.5 SP4. I usedSTEP 7 Professional 2010 SR2 and modify source as guide of MrJonasBengtsson. Then, you right click Setup.exe inSIMATIC_S7_STEP7_V55_SP4 and choose "Compatibility tab", tick "run this program in compatibility mode for" and choose "Windows 7".
|
2/15/2015 10:30 PM | |
Posts: 5 Rating: (2) |
I have installed Simatic STEP 7 V5.5 on windows 8.1, and it is very easy Follow this video https://www.youtube.com/watch?v=nD8l8MLqiW8 Download and install http://support.automation.siemens.com/WW/view/en/114358 http://www.angusj.com/resourcehacker/reshack_setup.exe http://www.instedit.com/ Edit ./Setup.exe/24/1/1033 Add the lines <supportedOS Id="{4a2f28e3-53b9-4441-ba9c-d69d4a4a6e38}"></supportedOS> <supportedOS Id="{1f676c76-80e1-4239-95bb-83d0f6d0da78}"></supportedOS> 4. Modify ./CD_2/Setups.ini under section OS. PlattformIDAllowed = 1;2;3 Add the lines Win8x64=1 Win8x64Exclude=SKU2;SKU3;SKU5;SKU8;SKU9;SKU10;SKU11;SKU12;SKU13;SKU14;SKU15;SKU16;SKU17;SKU18;SKU19;SKU20;SKU21;SKU22;SKU23;SKU24;SKU25;SKU47;SKU66;SKU67;SKU68 Win8x64Warning=SKU2;SKU3;SKU5;SKU8;SKU9;SKU10;SKU12;SKU13;SKU14;SKU15;SKU16;SKU17;SKU18;SKU19;SKU20;SKU21;SKU22;SKU23;SKU24;SKU25;SKU67;SKU68 5. Modify all msi-files with instedit Search for DLG_INSTALLATIONREQUIREMENTS_DISABLE_IGNORE. Change Action from Disable to Enable. Run ./Setup.exe |
6/4/2015 8:24 AM | |
Joined: 2/27/2012 Last visit: 4/17/2024 Posts: 6 Rating: (5) |
Sorry, but i think this thread is correct, because Graph is installed on Win8.1 :( |
8/5/2015 12:04 PM | |
Joined: 5/17/2013 Last visit: 4/30/2024 Posts: 14 Rating: (1) |
One more ICON! |
お疲れ様です, 毎度お世話になります |
|
8/5/2015 12:06 PM | |
Joined: 5/17/2013 Last visit: 4/30/2024 Posts: 14 Rating: (1) |
One More Icon again!!! |
お疲れ様です, 毎度お世話になります |
|
10/8/2015 9:52 PM | |
Posts: 1 Rating: (0) |
please tell me the what is the supported id of windows 8 32 bit and win8x32 Exclude and warning code.. Thanking you
|
10/12/2015 5:20 PM | |
Posts: 1 Rating: (0) |
Step 5. Modify all msi-files to enable the ingore-button on installation failures I Can not understand how to and where i modify in each of msi files. |
10/18/2015 1:48 PM | |
Posts: 2 Rating: (0) |
Hello. I cant downloaded that link. can you give me the mirror? thanks |
2/25/2016 9:31 AM | |
Joined: 4/22/2011 Last visit: 7/21/2023 Posts: 1 Rating: (0) |
Dear friend, Thank you for your directions. I tested it, it works akproster |
4/11/2016 10:43 PM |
|
Joined: 11/12/2015 Last visit: 2/22/2019 Posts: 4 Rating: (0) |
I'll try... |
1/25/2017 2:17 PM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Greeting All, Have a look on attached 5 Steps to install on Window 8.1 AttachmentDesktop.zip (735 Downloads) |
MS |
|
This contribution was helpful to1 thankful Users |
2/27/2017 8:31 AM | |
Joined: 1/27/2016 Last visit: 5/8/2024 Posts: 5 Rating: (0) |
hi team can someone take a snapshot of the msi file to manipulated as per point no 5 below on how to install s7 v5.5 in windows 8, am using Instead with no success. thanks in advance
5. Modify all msi-files to enable the ingore-button on installation failures (like installing on unsupported OS's). Use any software possible to manipulate MSI-files. E.g.InstEd. Search for DLG_INSTALLATIONREQUIREMENTS_DISABLE_IGNORE. Change Action from Disbale to Enable. |