5/17/2017 1:42 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Hello for all. Firstly, sorry for posting question with OMRON device. I need to connect RFID module omron V680S PDF and cpu S7-1511c-1 PN. I did the folowing: 1. Added GSD file to the project 2. Assigned ip, names 3. Downloaded all hardware to CPU Now in TIA portal online view there are not some "red" label with errors, but omron RFID is not working. The led on the body of RFID "LINK/ACT" is flashing continously , in the manual this flashing disribed like "flash during detects carrier" . The led RUN is always green. Perhaps, somebody met this device and worked normaly with it, pls, i hope you can give me advice With best regards,Dmitry. |
Last edited by: hadok at: 5/17/2017 1:43:34 PMLast edited by: hadok at: 5/17/2017 2:03:55 PM |
|
5/17/2017 3:21 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
Hi hadok, how do you know that it's not working? Are you reading and writing the I/O area of the RFID reader in OB 1? |
5/17/2017 4:50 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Led RUN is always green. If i try to send some bits from wath table (modify 0 to 1) nothing happens. Attachment0-02-05-0956e158d9e8b282b8b65ad5a8e2ef069e8814c73ab7055049dcbaaef1c56e7f_full.jpg (882 Downloads) |
5/18/2017 8:39 AM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Also would like to ask, is this addressing right? |
5/18/2017 1:21 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Yes, adresses are I 256.0 and Q256.0, so i think i must write in Q258.0 (offset 2) |
5/18/2017 1:28 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
On your opinion, command for the reading must be like here? |
5/18/2017 2:46 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
But why are you trying to set 257.0 to TRUE? From my understanding 257.0 is a reserved bit. |
5/18/2017 3:00 PM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
I did a mistake with addressing and have finded this addiction |
5/18/2017 4:08 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
Ah no problem. What about contacting the OMRON support? They should know about that behavior. I think I'm out of ideas. |
5/19/2017 11:26 AM | |
Joined: 4/28/2015 Last visit: 4/5/2024 Posts: 66 Rating: (4) |
Hello Qwei and all! I solved my problem. The trouble was in converting of addresses from siemens to Omron's tables of memory. For example, the bit READY is I257.0, the command EXE is Q257.0. I prepared picture with setings of TIA portal and converting of addresses, sorry for the big format of the picture. I hope it can be helpful for somebody. Manual for this RFID reader is on first message of this topic Also i made the sample project with CPU1511c and KTP600 Project v680s Omron - 1511c |
Last edited by: hadok at: 5/19/2017 11:34:43 AM |
|
This contribution was helpful to1 thankful Users |
11/6/2019 2:31 PM | |
Posts: 1 Rating: (0) |
Hi @Hadok Can you forward me your project ? I want to use OMRON V680S and i use TIA PORTAL V14. Please send me your project. Thank you. |
Follow us on