12/15/2020 5:43 PM | |
Joined: 11/8/2017 Last visit: 5/17/2024 Posts: 318 Rating: (175)
|
Hi, I've created a step by step guide that provides guidance on how to configure a customised alarm setup between Desigo PX and Desigo CC. The example used has 4 Event Lamps / Alarm Categories that can be named and coloured any way you want. The system is then configured to route alarms based on Alarm Priority to each of the Event Lamps / Alarm Categories. The example used will provide an understanding of the general concept and also how the configuration is done. This can then be modified as required and applied to different setups (however there are some limitations). I've attached the guide below, there are 9 pages to this, and there's also a video to demonstrate what the result should look like at the end. Hopefully it all makes sense. Regards, AttachmentCCCustomAlarming.zip (945 Downloads) |
This contribution was helpful to2 thankful Users |
1/8/2021 5:48 PM | |
Joined: 9/14/2013 Last visit: 7/16/2022 Posts: 24 Rating: (0) |
Hi CJ, That's really useful, thank you! Chris |
Follow us on