4/26/2024 6:26 PM | |
Joined: 2/4/2021 Last visit: 4/29/2024 Posts: 7 Rating: (0) |
You want to say: communication mode to TIA Portal and HMI? see picture I'll test it tomorrow |
4/27/2024 9:14 AM | |
Joined: 2/4/2021 Last visit: 4/29/2024 Posts: 7 Rating: (0) |
and second picture |
4/28/2024 6:53 AM | |
Joined: 3/30/2020 Last visit: 5/13/2024 Posts: 4501 Rating: (943) |
The Wincc is not finding the firmware version specified in the project. The last firmware version is V17. You can set inside Wincc the version of the HMI to be the same as the version in your device. Set the firmware of the device to V17 and install the HMI images on your PC. You need to decide if you want secure PLC to HMI communications: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on