3/19/2024 6:31 AM | |
Joined: 3/14/2008 Last visit: 5/22/2024 Posts: 2068 Rating: (928)
|
Hi, Do you have a ES+OS single station setup? |
If I could help you, you can use the RATE button. Thank you. |
|
3/19/2024 11:18 AM | |
Joined: 4/24/2019 Last visit: 5/21/2024 Posts: 13 Rating: (0) |
Hi Oreca. On this ES we configure with OSC (wincc appl. client) |
3/19/2024 11:28 AM | |
Joined: 3/14/2008 Last visit: 5/22/2024 Posts: 2068 Rating: (928)
|
Hi, In the following Link you can find the PCS7 Standard Architectures which shows several solutions and the license keys needed. See paragraph 5.1 for the setup OS client/OS server with Operator Control Monitoring on the ES. Please check if the required licences are available on your system. |
Last edited by: Jen_Moderator at: 03/19/2024 13:01:30Link optimized. If I could help you, you can use the RATE button. Thank you. |
|
3/19/2024 1:45 PM | |
Joined: 4/24/2019 Last visit: 5/21/2024 Posts: 13 Rating: (0) |
Based on the documentation all the related licenses available on this ES. not really know what happen as last few weeks it works fine. Maybe will try to transfer this OS Engineering license to another partition and test it again. Thanks for the link Oreca |
3/19/2024 1:58 PM | |
Joined: 3/14/2008 Last visit: 5/22/2024 Posts: 2068 Rating: (928)
|
You're welcome... You could also select the licenses in ALM and right click to check the status. It could be that one of them is defect. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on