3/14/2024 7:52 PM | |
Joined: 3/14/2024 Last visit: 4/15/2024 Posts: 1 Rating: (0) |
Hello friends I have a question for a updated of a PCS7 control system V7.1 at 9.1 It´s necessary buy all licences, from V7.1 to V8.2 – V8.x to V9.1 – V9.0 to V9.1? Or, I can realize a update of my license V7.1 to 9.1 with a only licence? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/15/2024 13:12:12New subject after splitting |
|
3/16/2024 7:21 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928)
|
Hi, You need to buy an upgrade license. This has to be done in two steps for your project:
See the following Industry mall link for more information: Update/Upgrade packages |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on