2/16/2024 10:55 AM | |
Joined: 5/6/2022 Last visit: 6/6/2024 Posts: 420 Rating: (83) |
Hi Sanket28, Have you tried to reset the panel to factory settings and reload the image version it had? Let's see if this way it is reconfigured and you can move the panel to Start? I leave you here how to reset the panel to factory settings: "How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"?" Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/22/2024 5:54 AM | |
Joined: 12/22/2018 Last visit: 5/30/2024 Posts: 83 Rating: (0) |
Thanks Murof ! Can you please explain what Flash drive of HMI does ? and what it contains ? |
Follow us on