9/2/2014 2:41 PM | |
Posts: 36 Rating: (2) |
Hallo, I was wondering if anyone can explain to me the difference between 'Paramaters' and 'Signals' when talking aboutprocess object options? I cannot find any hint on the only support (forum&product support) and in the offline help. There is only one close topic in this forum but it's stops when it becomes interessting. PCS7 Process Objects I want to do mass reconnecting (due to an updated MonDiL) as described here How can you use the process object view of the SIMATIC Manager to change block interconnections in the CFC? (Unfortunately, it does not work for outputs with more than one interconnection) I was playing with those attributes a bit it seems it makes a difference if I chose Parameter or Signal. In case of Parameter I can modify already connected I/Os but not in the case of Signal. Furthermore is shows me all signals in case of multiple interconnections. On the Signals tab, it is empty in case of multiple interconnection. See attachment for details. Can anyone explain that? thx Stefan AttachmentPOV-Parameters&Signals tabs + CFCs.pdf (219 Downloads) |
Follow us on