2/16/2024 4:01 PM | |
Joined: 1/31/2024 Last visit: 5/31/2024 Posts: 14 Rating: (0) |
Hi, I have a problem using the area button in WinCC V8.0 for a SCADA. I want to be able to see if there is an alarm going on in a page in the group display of the area button. But when I active one alarm in a page I cannot see it in the area button. Any solution? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: AntonioPio at: 02/16/2024 16:03:57Last edited by: The Helping Hand at: 02/19/2024 09:06:06New subject after splitting |
|
2/20/2024 10:32 AM | |
Joined: 8/3/2009 Last visit: 5/27/2024 Posts: 12984 Rating: (1654)
|
Hello AntonioPio i do not use this that much but there is a FAQ (Its a bit old but should act like the same) https://support.industry.siemens.com/cs/de/en/view/493670 Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/20/2024 11:29 AM | |
Joined: 1/31/2024 Last visit: 5/31/2024 Posts: 14 Rating: (0) |
Thanks, but I can choose the variable for the group display, but I can't find where it is modified. |
Follow us on