2/13/2024 8:02 PM | |
Joined: 4/1/2022 Last visit: 2/13/2024 Posts: 11 Rating: (0) |
I read the datasheet of 6ES7214-1BG40-0XB0 What does it mean by "Source/sink input = Yes" ? Does this mean I can use both sourcing and sinking configurations? Does this mean that 1M can be connected to either the positive or the negative of the power supply? (And of course, the inputs will be connected to the other terminal of the power supply). Or Does this specify the type of the device itself? So maybe Source/sink means that I should connect 1M only to the negative terminal of the power supply. And maybe for other devices, I may find Sink/Source which means that I should connect 1M only to the positive terminal of the power supply. I'm just trying to guess but I need a confirmation from you please. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/14/2024 08:25:36New subject after splitting |
|
2/14/2024 8:26 AM | |
Joined: 8/21/2014 Last visit: 5/22/2024 Posts: 959 Rating: (13) |
Closed cause question posted twice. The second thread with the subject What does (Source/sink input: Yes) mean in the datasheet of s7-1200 plc? is published within the conference SIMATIC S7-1200 Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on