12/31/2023 10:16 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928)
|
Hi, It seems it is not a problem with PCS7 but with third party software. Always respect the released Windows Operating system for PCS7 and generally VMworkstation is not tested by Siemens. What I could think of why it doesn't work with you is that you have a system with efficiency cores. By default VMware takes efficiency cores and this will deliver bad performance. There is a setting to enable VMware to use power cores only and this will boost the performance. You can find it very easily on the internet.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on