12/14/2023 10:59 AM | |
Joined: 6/25/2019 Last visit: 4/19/2024 Posts: 4 Rating: (0) |
Hi everyone, I have a problem with a redundand-server pcs7 project: The *.ldf is around 40 GB big and I already shrunk the database some time ago with the description in the FAQ: "How can you reduce the size of the transaction file (*.LDF) of the database of a WinCC project?" and it tells me to "Use the database without R at the end" but the log-data with the R at the end is the one that is huge (36 GB). What is the role of this database and is it OK to do the same procedure for it? Thank you. |
12/14/2023 11:46 AM | |
Joined: 3/14/2008 Last visit: 5/22/2024 Posts: 2068 Rating: (928)
|
Hi, The database with the _R means it is the database of the redundant server. I think this will be automatically cleaned up once you executed the procedure. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on