10/4/2023 7:11 PM | |
Joined: 6/11/2019 Last visit: 5/13/2024 Posts: 2199 Rating: (98) |
Hello W-VDB, welcome to the forum. After checking the input signal, you then have the option of filtering the input values with median averaging. This was also a topic in the German part of the forum (see here and here). Greetings Ella_68 (translated with Google) |
10/4/2023 7:57 PM | |
Joined: 12/18/2014 Last visit: 5/23/2024 Posts: 33099 Rating: (4085)
|
By a 0BA6? |
10/6/2023 2:36 PM | |
Joined: 6/11/2019 Last visit: 5/13/2024 Posts: 2199 Rating: (98) |
Hello W-VDB, The version with min-max module can be downloaded from the German forum. I'm attaching both variants, the ones for logos 6 and 8, as an attachment. Greetings Ella_68 AttachmentSpikefilter mit mediane Mittelwert (Logo 6 - 8).zip (340 Downloads) |
Follow us on