6/16/2023 3:49 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33162 Rating: (4097)
|
Which HMI have you? |
6/16/2023 3:50 PM | |
Joined: 6/15/2023 Last visit: 6/16/2023 Posts: 4 Rating: (0) |
KTP 700 Basic. |
6/16/2023 4:03 PM | |
Joined: 6/15/2023 Last visit: 6/16/2023 Posts: 4 Rating: (0) |
How can i do that? |
6/16/2023 4:06 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33162 Rating: (4097)
|
Which TIA version use you? Write it and I make you an example. |
6/16/2023 4:06 PM | |
Joined: 6/15/2023 Last visit: 6/16/2023 Posts: 4 Rating: (0) |
TIA Portal V18 |
6/16/2023 4:09 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33162 Rating: (4097)
|
I have only TIA V16. But when you the V16 version load in V18, you can upgrade it to V18. |
6/16/2023 5:35 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33162 Rating: (4097)
|
In attachment the example. AttachmentHours Counters Value to HMI.zip (404 Downloads) |
This contribution was helpful to1 thankful Users |
6/17/2023 3:45 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33162 Rating: (4097)
|
Is this solution okay for you? Or want you display only the hours without the decimal places? |
Follow us on