11/12/2021 3:11 PM | |
Joined: 9/16/2021 Last visit: 2/8/2024 Posts: 30 Rating: (2) |
Hello all, Currently we have a requirement that we need to change segement base object on circuit diagram report with another segment base object. Both the segement objects are same characteristcally. I have been able to identify the segment object using script and also able to delete it. What I do is I add the original co-oridnates in variable to use later to create the symbol for new Segment object.
But the problem is when I create the symbol using CreateSymbol Function, an object for Segement is added in hierarchy and the symbol on the report that is created is not correct and is not resizable. With Segment objects the objects is never created in the engineering project hierarchy but only symbol exist on report and that is resizable. Since the placed symbol is not desired, then that defeats the whole purpose of the activity. I am attaching screenshots for reference. If anybody can hel here or have a different solution then it will be really helpful Regards AttachmentSegment.zip (360 Downloads) |
Follow us on