2/24/2021 6:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, You need to use SMC 30 module to connect motor encoder connection & via Drive CLiQ SMC30 can be interface to CU250S. Please refer attached sheet for M23 HTL encoder pin connection details. Please refer manual https://support.industry.siemens.com/cs/de/en/view/109754294 chapter 8.6 for SMC 30 details. |
2/24/2021 7:35 AM | |
Joined: 5/16/2018 Last visit: 5/3/2021 Posts: 31 Rating: (0) |
Thank you for sharing. |
This contribution was helpful to1 thankful Users |
2/25/2021 3:28 AM | |
Joined: 5/16/2018 Last visit: 5/3/2021 Posts: 31 Rating: (0) |
Hi, Instead of using SMC 30 module, can I connect the motor encoder directly to the X2100 Encoder Interface on the CU250S-2PN? |
Follow us on