9/11/2020 4:59 PM | |
Joined: 8/25/2006 Last visit: 6/11/2024 Posts: 2207 Rating: (278)
|
Hello. What is LFE? Which card do you mean? What hardware do you use? |
9/13/2020 7:41 PM | |
Joined: 8/25/2006 Last visit: 6/11/2024 Posts: 2207 Rating: (278)
|
Hello. If you talk about data transfer from one CPU551 to another, then you need to have at least one communication module (CP50M0, CP50M1, CP51M1) which have buffer memory. Configure @GLOB FB to initialize buffer memory. On the CPU which is sender configure CTV FB, at its connector AT you should configure only name of connection (e.g. 'name') without address stage 1 and 2. Also cofigure required virtual connections, whch you want to send to another CPU. On the CPU which is reciever configure CRV FB with the same name at its connetor AR ('name'). Configure also the same virtual connections as you send from first CPU. But it is easier to use pointer-based communications via CRV_P/CTV_P. Also look at the manual, chapter 3.2.3 and 3.11.4. |
9/14/2020 10:30 PM | |
Joined: 6/2/2020 Last visit: 10/6/2023 Posts: 215 Rating: (0) |
Sir for reference, one attachment is attached. Please check, I want to do same type of connection in my TDC as I had used all free signals. Please describe in detail. |
Follow us on