Industry Online Support
Technical Forum
9/2/2005 9:39 AM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
Hello, there are several possibilies to solve your problem. You could use WinAC ODK V4.0 that provides a very fast "C" interface to the WinAC PLC. Another way is to use OPC. With Step 7 V5.2 and Simatic Net V6.1.1 you could use the Simatic Net OPC Server in the same PC Station with a WinAC Basis/RTX V4.0 Regards, Frank http://www.knoeller.de |
9/7/2005 1:42 PM | |
Joined: 8/31/2005 Last visit: 10/23/2023 Posts: 217 Rating: (40)
|
Hi Stan, check out this application: http://support.automation.siemens.com/WW/view/en/21447513 It is called "OPC: Mass Data Acquisition with an OPC Client in C# based on .NET". I think, this is exactly what you are searching for (just replace the S7-400 with the WinAC RTX). Greetings, Chris |
Last edited by: Chris at: 9/7/2005 1:46 PMGreetings, Chris |
|
Follow us on