Industry Online Support
Technical Forum
7/28/2011 4:43 PM | |
Joined: 7/15/2009 Last visit: 5/23/2024 Posts: 41 Rating: (1) |
Hi, and what happens if you set a velocity in "MC_MoveRelative" or "Absolute"at zero ? Is possible change current velocity of block "MC_MoveRelative" or "MC_MoveAbsolute" or"MC_MoveJog"when it is running? I´m thinking about application S7-1200 with PTO outputs for control ofservomotorsbut I´m not sure if is itpossible change velocity of current motion which was started from mentioned blocks. Thanks Splitted from Pausing PTO (MC on S7-1200). |
Last edited by: O_Moderator at: 7/29/2011 9:05 AMnew subject after splitting |
|
7/29/2011 9:06 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread motion control s7-1200 set velocity. Best regards O_Moderator |
Follow us on