12/14/2023 1:01 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078) |
Import of technical question from user grhntrmn via PM. Hi Ixo65 I saw that you are interested about HSP files. I need your help about hsp0185 v 3.0 v90. I am using TIA Portal v19. I have a project from TIA V17. When I try to upgrade the project from v17 to v19 I am taking error about that hsp0185 v90 v3.0 installation requires. I installed last HSP verison for V19. But there was no HSP0185 in that. I am sharing the screen image for you see Can you share ıf you have hsp0185 for TIA V19 or can you help me if you can do anything ? |
This contribution was helpful to1 thankful Users |
12/14/2023 1:04 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
not released yet, you must weit a few weeks for the HSP'S |
12/14/2023 1:07 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078) |
https://support.industry.siemens.com/cs/attachments/72341852/TIA_Portal_V17_HSP.zip |
12/14/2023 1:10 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
he need it for V19 not v17 or? |
12/15/2023 5:21 AM | |
Joined: 10/3/2021 Last visit: 1/10/2024 Posts: 2 Rating: (0) |
Hi, I need V19 HSP for v90 pn v3.0. As you said, I should wait a few weeks for HSP 0185. Thanks again. |
12/17/2023 3:55 AM |
|
Joined: 3/21/2016 Last visit: 1/26/2024 Posts: 1 Rating: (0) |
V19版本HSP0185 |
3/9/2024 9:43 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33003 Rating: (4078) |
Support Packages for the hardware catalog in the TIA Portal (HSP) |
Follow us on