1/8/2024 1:21 PM | |
Joined: 7/19/2022 Last visit: 6/5/2024 Posts: 363 Rating: (61) |
Hello Manthan patel, The SM1231 module has analog inputs, not outputs. The analog output module is the SM1232. If you want to connect the SM1232 to an S7-300 you will simply have to take the analog output pins of the SM1232 and connect them according to the 2-wires configuration indicated here: SIMATIC S7-300 SM331; AI 8x12 Bit Getting Started part 1: 4 -20mA |
If this Information really helps, you could use the Rate function |
|
Follow us on