8/9/2023 6:48 AM | |
Joined: 10/11/2006 Last visit: 6/4/2024 Posts: 5856 Rating: (793)
|
Hello, check, if it is possible to move the motor with drive control pannel of V-Assistant. Check the torque limits. For TO conficuration there is a example. https://support.industry.siemens.com/cs/de/de/view/109743917 Please check the encoder settingts and the reference values at the TO. They must suit to the settings in the drive. P2000; p29418; p29419; ... |
With best regards, |
|
8/9/2023 8:27 AM | |
Joined: 12/26/2021 Last visit: 12/4/2023 Posts: 5 Rating: (0) |
Thanks All settings have been checked and everything is correct. When I use Telegram 3 alone, it works fine.When using Telegram 750, servo motor movement and speed cannot be controlled. I think, other parameters need to be adjusted, which I don't know about |
Last edited by: mehranlll at: 08/09/2023 08:33:40 |
|
8/14/2023 4:50 AM | |
Joined: 12/26/2021 Last visit: 12/4/2023 Posts: 5 Rating: (0) |
Hello Thank you for your response |
Follow us on